KEMET Advances Automotive Grade Polymer Solutions for Avionics and Automotive Applications
T598 offers high reliability and more board space for harsh environment design requirements
KEMET, part of the Yageo Group and leading global supplier of electronic components, today announces the technological advancements of its tantalum polymer automotive T598 capacitor series. This series fulfills the growing need for increased reliability of tantalum polymer capacitors beyond currently available commercial grade solutions for both commercial avionic applications and automotive applications, such as advanced driver-assistance systems (ADAS).
Meeting the AEC-Q200 automotive standard and part of the KO-CAP® automotive series, the T598 capacitor offers higher capacitance, volumetric efficiency, and ESR stability under harsh environmental conditions. Building from the success of the T598 series in the automotive, industrial, and telecommunication industries, KEMET’s engineering team advanced the series for use in the defense and aerospace industry. For the T598’s expansion into commercial avionics technologies, a special H termination (Sn/Pb) and a surge current option per MIL-PRF-55365 standards was added. The series fully supports avionic applications that require high capacitance and less board space, as tantalum polymer technologies exhibit less capacitance roll-off than MnO2-based solutions.
Advancements in the T598 series make it an exceptional automotive grade solution for DC-DC 3.3V and 5V power lines in ADAS. Its new maximum capacitance offering in EIA3528-21 to 150µF 6.3V and high volumetric efficiency supports the miniaturization trend and reliability requirements in the growing ADAS market. According to a June 2020 report from Prismark Partners*, this market is expected to grow at a CAGR of 15.5% from 2019 to 2024 and reach USD 27 billion by 2024.
The T598 series is available immediately via KEMET distributors. To learn more about its capabilities and applications, visit https://ec.kemet.com/polymer-automotive/.
*Source: Electronics Supply Chain Reporter Q2 2020, Prismark Partners LLC, June 2020
About KEMET
KEMET, a subsidiary of Yageo Corporation (TAIEX: 2327) and part of the Yageo Group, helps our customers build tomorrow with the broadest selection of capacitor technologies in the industry, along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. With over 100-years of making the world a better, safer, and more connected place to live, our vision is to be the preferred supplier of electronic component solutions demanding the highest standards of quality, delivery and service. Additional information about KEMET can be found at www.kemet.com.
Stay connected to KEMET on Facebook, LinkedIn, Twitter, Instagram and YouTube.
About Yageo Group
Yageo Group is a global provider of passive component solutions offering the broadest selection of passive component technologies from some of the industry’s most recognized brands. With a leading portfolio of chip resistors, polymer, tantalum, MLCC, film, and aluminum electrolytic capacitors, circuit protection devices, magnetics, antennas, sensors, and actuators, as well as global production and sales capabilities designed to meet the diverse requirements of customers and a full range of end-market segments.