KEMET Introduces Space-Saving Film Capacitor for Automotive, Industrial, Consumer, and Energy Applications
R52, an X2 EMI Suppression series, is a first-to-market solution that offers high capacitance, extended stability in harsh environments, more board space, and lower costs for engineers
KEMET, part of the Yageo Group and leading global supplier of electronic components, today announces its new R52 series of compact polypropylene film X2 EMI (electromagnetic interference) suppression capacitors. This series fulfills the growing need of automotive, industrial, consumer, and energy applications that require a smaller, high-capacitance X2 class solution for suppressing EMI. While the R52 series offers capacitance values up to 22µF, 85/85 THB Class IIB classification, and long-life stability in harsh environmental conditions, its volume on average is 60% smaller than other X2 solutions with the same range of capacitance values in the market. These features alone position R52 as an exceptional X2 class solution that addresses size, capacitance, and reliability challenges for design engineers across multiple industries.
Meeting the AEC-Q200 automotive standard, the R52 series can be used in DC/DC converters within on-board battery charger systems found in electric and hybrid vehicles. Its unique design features are well-suited for industrial and consumer applications, including EMI filtering for VFD (variable frequency drives) and LED (light emitting diode) drives. This series is also positioned to support applications with elevated energy densities, such as compact capacitive power supplies. R52 capacitors are constructed to meet high standards of reliability that are required for smart grid hardware that is often located in limited access areas where regular service is not available.
Currently available solutions comparable to the R52 series have either larger dimensions or require capacitors in parallel in the design. These solutions require more PCB (printed circuit board) space, resulting in higher costs and lower reliability. The R52 series offers the highest capacitance density with a smaller footprint when compared to similar X2 film solutions available in the market.
The R52 series is available immediately via KEMET distributors. To learn more about its capabilities and applications, visit https://ec.kemet.com/film.
About KEMET
KEMET, a subsidiary of Yageo Corporation (TAIEX: 2327) and part of the Yageo Group, helps our customers build tomorrow with the broadest selection of capacitor technologies in the industry, along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. With over 100-years of making the world a better, safer, and more connected place to live, our vision is to be the preferred supplier of electronic component solutions demanding the highest standards of quality, delivery and service. Additional information about KEMET can be found at www.kemet.com.
Stay connected to KEMET on Facebook, LinkedIn, Twitter, Instagram and YouTube.
About Yageo Group
Yageo Group is a global provider of passive component solutions offering the broadest selection of passive component technologies from some of the industry’s most recognized brands. With a leading portfolio of chip resistors, polymer, tantalum, MLCC, film, and aluminum electrolytic capacitors, circuit protection devices, magnetics, antennas, sensors, and actuators, as well as global production and sales capabilities designed to meet the diverse requirements of customers and a full range of end-market segments.