Transient Liquid Phase Sintering (TLPS) Image

Term:

Transient Liquid Phase Sintering (TLPS)

Definition:

Transient Liquid Phase Sintering (TLPS) is the low-temperature reaction of a low melting point metal or alloy with a high melting point metal or alloy to form a reacted metal matrix.

TLPS forms a metallurgical bond between two surfaces. Depending on the allow, TLPS may have a re-melt temperature in excess of 600°.

More information regarding TLPS can be found in this presentation on the Development and Characterization of High-Temperature MLCCs using Transient Liquid Phase Sintering (TLPS).

Added on:

Monday, October 5th, 2015